AXIS#.ACTIVE

Description

AXIS#.ACTIVE reads the enable status of an axis as follows:

  • AXIS#.ACTIVE = 0 axis disabled
  • AXIS#.ACTIVE = 1 axis enabled
  • AXIS#.ACTIVE = 3 axis is in dynamic brake mode

There is no state 2.

When the drive is in state 3, the drive display shows a gray background when disabled and a green background when enabled. If either of the axes is in state 1 (enabled), the Parameter Load/Save view does not allow you to download a parameter file.

If an axis is not enabled (.ACTIVE is 0), but AXIS#.EN is 1 and the hardware enable is high,read the value of AXIS#.DISSOURCES to query the reason that the drive is not enabled.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

0, 1, 3

Default Value

N/A

Data Type

Integer

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5003

1

5003 (0x138b)

AXIS1.ACTIVE

Unsigned8

Read Only

Yes

70539

2

5003 (0x138b)

AXIS2.ACTIVE

Unsigned8

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.ACTIVE

5003

Unsigned8

Read Only

-

Related Topics

Enable/Disable

AXIS#.EN ,AXIS#.DISSOURCES